Pull changes

Pull changes

Pull changes to view updates and conflicts between the remote and local repositories. Use Pull preview to accept updates and resolve conflicts.
TIP: When there are changes to pull from the remote repository, the message
Remote changes available to pull
appears in the status bar and the
Pull from remote
icon displays a blue number with the number of commits to pull. For example,
Pull from remote
indicates that there is one commit that is ready to pull.
Prerequisites
  • Configure your user identities for version control providers. See Configure version control.
  • If prompted, commit local changes before pulling remote changes.
  1. To pull changes
  2. In the open project, select
    Pull from remote
    .
    Changes and conflicts between the local project and the project in the remote repository appear highlighted in
    Pull preview
    . For more information, see Pull preview.
    TIP: A conflict may occur if a property value in both the remote project and the local project has changed. A conflict may also occur if an object is removed in one version of the project and the same object is modified in the remote repository. Highlighted conflicts display changed values and removed objects that are crossed out. The number of conflicts appears in the status bar.
  3. (optional) At the top of
    Pull preview
    , select the content to view:
    • All
      . All project content in both the local and remote projects.
    • Updates
      . Only changes in the local and remote projects.
    • Conflicts
      . Only conflicts between the local and remote projects.
  4. Expand a highlighted conflict to display the values in conflict.
  5. (optional) At the top of the preview, select
    Sort descending
    to navigate and expand the next conflict or
    Sort ascending
    to navigate to the previous conflict.
    TIP: An icon in a row in
    Pull preview
    indicates:
    • Preview conflicts
      A conflict exists between the local and remote repository.
    • Preview resolved
      A conflict was resolved by selecting either the local or remote change in the row.
    • Preview changes
      A change exists in the local or remote repository.
    • Preview additions
      An object was added.
    • Preview deletions
      An object was removed.
  6. In each highlighted row, select the version of content to keep:
    • Individual local change. In a highlighted row, select the local change
      Local history
      on the left.
    • Individual remote change. In a highlighted row, select the remote change
      Remote history
      on the right.
    • All local changes. At the top of the preview, select
      Take all local
      .
    • All remote changes. At the top of the preview, select
      Take all remote
      .
  7. Select
    Accept
    to accept the selected changes, or select
    Cancel
    to reject all of the conflicts in the remote project and retain the values in the local project.
The project opens and the message
The project is synchronized
appears in the status bar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal