Create the System object

Create the System object

The
System
object allows users to view and configure certain system variables, such as the date and time, device, display, and application settings for the
FTOptixApplication
.
Create one
System
object per project.
  • In
    Project view
    , right-click
    Model
    and then select
    New
    All
    System
    System
    .
    System1
    appears in
    Project view
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal