Configure an XY chart

Configure an XY chart

Configure an XY chart to visualize data.
  1. In
    Project view
    , in
    UI
    , right-click a container and then select
    New
    Data controls
    XY chart
    .
  2. (optional) In
    Properties
    , set:
    • Zoom
      . The zoom level of the chart.
    • Center X
      . X coordinate in relation to which to center the chart.
    • Center Y
      . Y coordinate in relation to which to center the chart.
    • Key visible
      . Show or hide the legend of the pens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal