PDF Viewer

PDF Viewer

Displays a PDF file at runtime.

Operation

The PDF viewer can display either:
  • A local PDF file stored in the project directory
  • A PDF file stored on a remote server
    PDF viewer supports these protocols for displaying remote PDF files:
    • http
    • https

Use case

Use embedded PDFs to provide the end users with quick access to technical documentation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal