Screen

Screen

Use screens to group objects that comprise a specific interface.

Screen types and instances

For optimal project maintainability, create screen object types and then use them with panel loaders or navigation panels. This allows you to modify all screen instances by editing the parent screen type.

Screens folder

Rockwell Automation
recommends creating screen types in the
UI
Screens
folder in
Project view
. You can also create screen types in different nodes of your project, for example in the UI folder.
Each new project contains an empty
Screens
folder.
TIP: If the project does not contain a
Screens
folder, see Add a Screens folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal