Make a graphic object movable

Make a graphic object movable

Make a container or drawing object movable so that the user can drag the object at runtime.
TIP: You can create movable dialog boxes and other floating interface elements.
  1. In
    Project view
    , select an object.
  2. In
    Properties
    , set
    Move target
    :
    • None
      . Object does not move as you drag the object at runtime.
    • Self
      . Object moves as you drag the object at runtime.
    • <AncestorObject>
      . Ancestor and descendant objects move as you drag the movable object at runtime.
Example
Consider this scenario:
  • The blue rectangle object is a child of the orange rectangle object.
  • The
    Move target
    of the blue rectangle is set to the orange rectangle.
  • At runtime, if you drag the blue rectangle, both blue and orange rectangles move.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal