Change objects order

Change objects order

Move selected objects in front of or behind other objects in the editor.
  1. In
    Project view
    , double-click a container or select
    Editor
    .
    The editor opens a separate tab.
  2. Select the object to move.
    TIP: To select multiple objects, hold
    Ctrl
    and select multiple objects.
  3. In the editor toolbar, select the button to move the object in relation to other objects:
    • Send to back
      . Send the object behind all objects in the editor.
    • Send backward
      . Send the object behind the next object in the editor.
    • Bring forward
      . Send the object in front of the next object in the editor.
    • Bring to front
      . Send the object in front of all objects in the editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal