Graphic objects

Graphic objects

Use predefined graphic objects to add visual components to
FactoryTalk Optix Applications
. Use presentation engines to display the application UI at runtime on different viewports.

Predefined graphic objects

FactoryTalk Optix Studio
includes different categories of predefined graphic objects to add to your project. You can customize the predefined graphic objects by editing their properties and by creating, editing, and modifying style sheets. You can also create custom graphic object types.
For more information, see Predefined graphic objects.

Graphic objects management

In
Project view
and in the editor, create, duplicate, edit, and set properties of graphic object instances and graphic object types.
For interface overview, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal