Creating projects

Create a
FactoryTalk Optix
project and the application logic for the project. Add content to the project that includes graphic objects and dynamic links to have those objects display values to visualize your system at runtime.
Perform, display, and record changes to your system using events, alarms, and reports. Add version control to a project as you make changes so that you can revert to a previous version of the project.
Assign roles and create security authentication for your project. Add different locations and languages to the project to  impact the content shown at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal