System requirements
Use these system requirements to determine whether your computers can run
FactoryTalk® Optix™
and FactoryTalk Optix Applications
.Hardware requirements for FactoryTalk Optix Studio desktop editor
FactoryTalk Optix Studio desktop editor
For optimal performance of
FactoryTalk Optix Studio desktop editor
, the computer should meet or exceed these hardware requirements:
- Intel Core i5 Standard Power processor (i5-8xxx)
- 8 GB of RAM memory
- 20 GB free hard disk space
Software requirements for FactoryTalk Optix Studio desktop editor
FactoryTalk Optix Studio desktop editor
- Microsoft® Windows 10 (x64) or Microsoft Windows 11 (x64)
- An external code editor to develop custom C# NetLogic codeNOTE:Rockwell Automationrecommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
Software requirements for FactoryTalk Optix Studio web editor
FactoryTalk Optix Studio web editor
- A web browser that supportsFactoryTalk® Hub™
Hardware requirements for FactoryTalk Optix Applications
FactoryTalk Optix Applications
Hardware requirements for
FactoryTalk Optix Applications
may vary depending on the application and the type of device that runs the application.Software requirements for FactoryTalk Optix Applications
FactoryTalk Optix Applications
- Windows 10 (x64), Windows 11 (x64), or Ubuntu 22 (x64)
NOTE:
FactoryTalk Optix and FactoryTalk Optix Applications can run inside hypervisors such as VMware® version 15 or higher. For compatibility reasons, software rendering is used by default.
NOTE:
FactoryTalk Optix Applications are supported on closed Rockwell Automation devices that include OptixPanels and Embedded Edge Compute which run Yocto (ARM64).
Provide Feedback