Array editor

Use the array editor to modify the values of array variables.
Array editor
Array editor items
Item
Name
Description
1
Add
Add
Adds a cell to an unconstrained array.
2
Delete
Removes a cell from an unconstrained array.
3
Array cells column
Lists array cells.
4
Array values column
Lists editable array cell values.
TIP:
If the array lists colors, you can select the color preview to open the color selector.
You can create dynamic links in cell values and make the parent array index dynamic. For more information, see Create dynamic links.
5
Apply
button
Applies changes to the array values and closes the editor.
6
Cancel
button
Cancels changes to the array values and closes the editor.
7
Open in tab
button
Opens the array editor in the central pane.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal