Spin box

Increase/decrease a numerical value using buttons or keyboard.
BrowseName
SpinBox
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Value
Value
Value displayed and possibly changed by the user.
Minimum value
MinValue
Minimum value displayed on the Y axis.
Maximum value
MaxValue
Maximum value displayed on the Y axis.
Increment
Increment
Added or subtracted value (for example, 1, 0.1, or 0.01) using buttons.
Input format
Format
Editable
Editable
Enable/disable the change of the value directly in the chart.
Show buttons
ShowButtons
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Text color
TextColor
Color of the text to display.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

Modified value
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal