Features

The following are the features in the FactoryTalk Edge Manager 1.00.00 Release:
  • Edge Devices Fleet Management
    FactoryTalk Edge Manager can manage the edge devices as a fleet, while offering the flexibility of extendible configuration setup templates for identical equipment or custom machinery deployments. This enables configuration a software maintenance update, schedule it and then deploy to the entire fleet with a single action.
  • Extendible App Marketplace
    FactoryTalk Edge Manager offers an application marketplace that supports orchestration of multiple applications— running in virtual machines (VMs), containers or clusters—on one industrial computer. Users can push software application updates to multiple edge devices simultaneously.
  • Affordable Access to Data
    The first app from Rockwell Automation in the public marketplace is FactoryTalk Edge Gateway™ and is included with every managed edge device to help customers break down their data silos. The latest capabilities in FactoryTalk Edge Gateway will make it easier to configure devices with a cloud-hosted tool to manage data sources, data models, and data egress.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal