Edit a data source

Edit a data source to modify the settings.
TIP:
Models using the edited data source automatically update to reflect the changes. Redeploy applications consuming the impacted models to reflect the modifications done to the data source.
To edit a data source
  1. Select
    Data Flow
    >
    Data Sources.
  2. (optional) From
    Configure Data Sources
    , filter the list of data sources.
  3. Select
    Edit
    for the required data source.
  4. From
    Configure Data Source
    , modify the settings for the data source.
  5. Select
    Save
    to edit the data source.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal