Add a data source from an OPC DA Device

NOTE:
The OPC DA device is supported by standalone version only.
Add data sources from OPC DA devices to populate a namespace and collect data from data tags.
The
OPC DA Device
data source is compatible with the OPC DA Access (DA) driver.
To add a data source from an OPC DA Device
  1. Select
    Data Flow
    >
    Data Sources
    , and from
    Configure Data Sources,
    add a data source.
    • To add the first data source, select
      Add Data Sources
      .
    • To add a subsequent data source, select
      Add
      .
  2. Enter the
    Name
    and then from
    Tags and types defined in (data browse path type),
    select
    OPC DA Device
    .
    • The name must contain only letters, numbers, and hyphens.
  3. From
    Driver for browsing
    , select the OPC DA Access (DA) driver.
  4. Perform one of these actions:
    • Enter the
      Browse path
      in the following format. Use "+" in place of space to enter the path. For example: To enter "RSLinx OPC Server", type "RSLinx+OPC+Server".
      • For remote servers:
        Computer_Name/Server_Identifier:Channel.Device (i.e. Computer1/Kepware.KEPServerEnterprise:Channel1.Device1)
      • For local servers:
        Server_Identifier:Channel.Device (i.e. Kepware.KEPServerEnterprise:Channel1.Device1)
    • Select the path from
      OPC Local Servers
      drop-down list.
      OPC Local Servers
      drop-down list contains only Local OPC servers.
  5. (optional) To generate the namespace, select
    Auto-populate namespace
    .
  6. Perform one of these actions:
    • Select
      Use browse path for data collection
      .
    • From
      Driver for Collectio
      n, select the OPC DA Access (DA) driver for the data collection path and enter the collection path.
  7. Select
    Save
    to add the data source.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal