Data Ingress

Data ingress is implemented as data sources in
FactoryTalk Edge Gateway
. Data sources allow an OT engineer to identify data critical for analysis. Use
FactoryTalk Edge Gateway
to configure a pathway to collect data from these sources:
  • Studio 5000 Logix Designer
    project file (.acd)
  • Studio 5000 Logix Designer
    controller
  • FactoryTalk® Live Data
    shortcut
  • Drive/IMC device
  • OPC DA device (In distributed version, OPC DA data can be obtained via the FTLD shortcut using the FTLDR connector)
  • KEPServer Enterprise
    device for third-party-data connectivity (standalone version only)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal