Verification

  1. Verify successful installation. Refer to Verification Steps (Application Installation).
  2. Login as a DataView Admin User. On the Usage Info page, user can view the list of old licenses and the old design users migrated.
  3. Logout and login as Design User.
  4. Under the Content tab, user can view the old storyboards and under the Connections tab, user can view the old connections.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal