Elasticsearch Logs
The Elasticsearch Logs are enabled by default and are available in the path specified while installing Elasticsearch:
<<Elasticsearch Installation Directory>> ProgramData>Elastic>Elasticsearch>logs
TIP:
Unhide the hidden files. In the View menu, select the [Hidden items] checkbox. The hidden files display.
Hidden Files

Elasticsearch Log

Provide Feedback