Create Database

  1. Open the pgAdmin4 application. Click [Servers] and provide the master admin password.
    pgAdmin Application
  2. Double-click [PostgreSQL 13] and provide the password to open pgAdmin.
    PostgreSQL Password
  3. Right-click [Databases], click [Create] and then click [Database] to create a database manually as shown in the following image.
    Create a Database
  4. Provide the database name and click [Save] to create the database.
    Database Name
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal