Supported dongle types

Binding an activation to a dongle's serial number allows the dongle to activate software on any computer that the dongle is attached to.
Using a plug and play dongle with storage capacity allows
FactoryTalk Activation Manager
to detect the dongle automatically and provide the option of downloading activation files to it. The dongle can then be connected to any computer and used to activate software.
Each dongle is labeled:
  • CodeMeter dongles are labeled
    CmStick
    or
    CmCard
    .
  • FlexNet dongles are labeled
    FlexNet, Flexera, HASP
    , or
    FLEXid
    .
FactoryTalk Activation Manager
supports the following activation dongles:
Catalog Number
Name
Storage
9509-USBDONG2
FlexNet
8 GB
9509-CMSTICKC
CodeMeter CmStick Compact
None
9509-CMSTICK8
CodeMeter CmStick
8 GB
9509-CMSDCD4
CodeMeter CmCard SD
4 GB
In some cases, a product's activation requires a specific dongle type. The error message
Different dongle type needed
indicates that the dongle in use does not support the activation of the product. The message indicates
the type of dongle required, FlexNet or CmStick. Identify the correct dongle type and plug it into the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal