Product does not start properly after borrowing activations

Possible cause and solution:
  • An incorrect set of activations were borrowed.
    Click
    Manage Activations > Find available activations
    and view the list of available activations. If the activations needed are not available, return the previously borrowed activation and borrow the required set.
  • The activations were borrowed before the latest update of
    FactoryTalk Activation Manager
    .
    If the activation was borrowed using an earlier version of
    FactoryTalk Activation Manager
    , return the activation, update
    FactoryTalk Activation Manager
    , and borrow the activation again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal