Inaccurate display of borrowed information

View borrow details from
Find Available Activations
by selecting the number in the
Borrowed
column.
However, upon restart, the
Borrow Details
dialog box on the Activation Server will show an inaccurate expiration date for the
FactoryTalk Activation
Service on the
FactoryTalk Activation
Server of the borrowed activation. The expiration date will be based on the time the
FactoryTalk Activation
Service was restarted instead of the time when the activation was borrowed. This behavior does not affect when the borrowed activation will expire and automatically returned. The initial term of the borrow will be honored. Only what displays in the
Borrow Details
dialog box is inaccurate. Inaccurate expiration dates and times might appear on client computers, also, if the
FactoryTalk Activation Manager
application is open when the Activation Server is rebooted.
Additionally, if a borrowed activation is renewed, in
Find Available Activations
on the Activation server, the numbers in the
In use
and
Borrowed
columns are changed from 1 to 0. The borrowed activation will be returned as normal. Only what displays in
In use
and
Borrowed
is inaccurate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal