Disk drive binding is not available for selection

Possible cause and solution:
  • The computer may have more than one hard disk drive.
    The only hard disk drive binding listed is for the hard disk drive that the computer uses to boot up. Use that binding or bind the activation to the Ethernet MAC ID.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal