Activation checkout is denied

Possible cause and solution:
  • All available activations are checked out.
    Wait until an activation is returned or contact
    Rockwell Automation
    technical support to purchase additional activations.
  • The activation file was modified.
    Rehost the activation file. Modified activations files are no longer valid. In these instances, get a new activation.
  • The activation file contains an invalid license.
    Renew the activation file. If the license is invalid, a new license file must be granted from the activation server.
  • The options file restricts access to activations.
    Update the options file to enable the required access.
  • The activation is not available on the server providing activations.
    Update the Path to Activations to include the activation server that is hosting the activation needed.
    TIP: Additional information about denied activations may be available in the activation server log file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal