WriteReturnUpdate

Use the
writeReturnUpdate
command on the source computer to write return data to a transport data file created using
selectReturnSource
. This file can then be used with the
importReturn
and
confirmReturn
commands to complete a return operation without a server connection.
IMPORTANT: A disconnected return operation is only supported by CodeMeter activations.
These options are required:
  • '-d, --disconnected'
Usage: writeReturnUpdate [options]
This table describes the command options.
Option
Description
-d|--disconnected
The filepath for the data transport file.
Example: '-d:C:\Users\jdoe\Documents\ReturnByFileData.xml'
-?|-h|--help
Show help information.
-v|--verbose
Use this option to turn on trace messaging.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal