WriteRenew

Use the
writeRenew
command to write the renew data for all local activations to the specified transport data file.
This is the first step in the disconnected renew workflow. The
general --disconnected
option, which specifies the transport data file, is required.
Usage: writeRenew [options]
This table describes the command options.
Option
Description
-d|--disconnected
Use this required option to support disconnected workflows (get, rehost, and renew). You can specify a file spec for the data transport file. If you do not specify the file spec, a default file spec is used.
Example: '-d:C:\Temp\TransportFile.xml'
Note:
'-d C:\Temp\TransportFile.xml' results in a parsing error. You must insert either ':' or '=' when specifying the data transport file.
Note:
The file spec must be for an xml file and therefore have an .xml file extension.
-v|--verbose
Use this option to turn on trace messaging.
-f|--forcedOverwrite
Use this option with the -d|--disconnected option. When you include this option, the specified disconnected transport data file will be overwrritten if it exists.
Example: 'getbindings -d:C:\Temp\TransportFile.xml -f'
Note: This option can only be used with the commands getbindings, selectRehost, and writeRenew.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal