UpdateRehost

Use the
updateRehost
command to take the rehost data from the specified transport data file, communicate with the
Rockwell Automation
web service and write the rehost update data back to the transport data file.
This is the second step in the disconnected rehost workflow. Run this command from a computer that is connected to the Internet. The
general --disconnected
option, which specifies the transport data file, is required.
Usage: updateRehost [options]
This table describes the command options.
Option
Description
-d|--disconnected
Use this required option to support disconnected workflows (get, rehost, and renew). You can specify a file spec for the data transport file. If you do not specify the file spec, a default file spec is used.
Example: '-d:C:\Temp\TransportFile.xml'
Note:
'-d C:\Temp\TransportFile.xml' results in a parsing error. You must insert either ':' or '=' when specifying the data transport file.
Note:
The file spec must be for an xml file and therefore have an .xml file extension.
-v|--verbose
Use this option to turn on trace messaging.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal