SelectBorrowDestination

Use the
selectBorrowDestination
command on the destination computer to create a transport data file containing information about the destination binding. The resulting file can be used with the
selectBorrowSource
,
importBorrow
, and
confirmBorrow
commands to perform a borrow operation without a server connection.
IMPORTANT: A disconnected borrow operation is only supported by CodeMeter activations.
These options are required:
  • '-d, --disconnected'
  • '-db, --destinationbinding'
Usage: selectBorrowDestination [options]
This table describes the command options.
Option
Description
-d|--disconnected
The filepath for the new data transport file.
Example: '-d:C:\Users\jdoe\Documents\BorrowByFileData.xml'
-db|--destinationbinding
The destination binding identifier. This is the binding where the activation will be borrowed to.
Example:'-db 130-3618734'
In this example, the value is the CodeMeter container id/mask-serial number used when borrowing a CodeMeter activation.
-?|-h|--help
Show help information.
-v|--verbose
Use this option to turn on trace messaging.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal