Renew

Use the
renew
command to renew an activation. Only activations whose serial number has been renewed in the
Rockwell Automation
subscription portal are renewable.
This option is required:
  • '-sn, --serialnumber'
This parameter is optional:
  • '-b, --binding'
These options can be included multiple times:
  • 'sn, --serialnumber'
Usage: renew [options]
This table describes the command options.
Option
Description
-v|--verbose
Turns on trace messaging.
-sn|--serialnumber
Required: The 10-character, alpha-numeric serial number provided in the Activation certificate.
You can include multiple serial numbers.
Example: '-sn 5555566778'
-b|--binding
Optional: The binding identifier.
Use the
GetBindings
command to determine possible binding indentifiers.
Example: '-b 130-2526232760'
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal