ConfirmRehost

Use the
confirmRehost
command as the fourth and final step in the disconnected rehost workflow. You must run this command from a computer that is connected to the Internet. This command takes the confirmation rehost data from the specified transport data file and sends it to the Rockwell web-service. The Rockwell web-service then increments the activation install count for the activation that has been returned.
The
general --disconnected
option, specifying the transport data file, is required.
Usage: confirmRehost [options]
This table describes the command options.
Option
Description
-d|--disconnected
Use this required option to support disconnected workflows (get, rehost, and renew). You can specify a file spec for the data transport file. If you do not specify the file spec, a default file spec is used.
Example: '-d:C:\Temp\TransportFile.xml'
Note: '-d C:\Temp\TransportFile.xml' results in a parsing error. You must insert either ':' or '=' when specifying the data transport file.
Note: The file spec must be for an xml file and therefore have an .xml file extension.
-v|--verbose
Use this option to turn on trace messaging.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal