Borrow

Use the
borrow
command to borrow an activation.
These options are required:
  • '-fn, --featurename'
  • '-fv, --featureversion'
  • '-sb, --sourcebinding'
  • '-db, --destinationbinding'
  • '-bt, --borrowterm'
NOTE:
Multiple options can be used so long as an equal number of other required options are also entered. For example, two -fn options can be entered so long as two -fv, -sb, -db, and -bt options are also entered.
The multiple options are order dependent. The first -fn value is used with the first -fv, -sb, -db, and -bt values. The second -fn value is used with the second -fv, -sb, -db, and -bt values, and so on.
Usage: borrow [options]
This table describes the command options.
Option
Description
-v|--verbose
Use this option to turn on trace messaging.
-fn|--featurename
The feature name of the activation to borrow.
You may enter multiple feature names so long as an equal number of other required options are also entered.
Example: 'RS5K_600.EXE'
-fv|--featureversion
The feature version of the activation to borrow.
You may enter multiple feature versions so long as an equal number of other required options are also entered.
Example: '1.00'
-sb|--sourcebinding
The source binding identifier. This is the binding where the activation will be borrowed from.
You may enter multiple source bindings so long as an equal number of other required options are also entered.
Example: '-sb fnp'
In this example, 'fnp' indicates that the activation is an fnp/flexera activation.
Note: The first available activation with the given feature name will be borrowed.
Example: '-sb <computername>:130-3618734'
CodeMeter container ID/mask-serial number used when borrowing a CodeMeter activation, where <computername> is name of a computer or an IP address.
-db|--destinationbinding
The destination binding identifier. This is the binding where the activation will be borrowed to.
You may enter multiple destination bindings so long as an equal number of other required options are also entered.
Example: '-db fnp'
In this example, 'fnp' indicates that the activation is an fnp/flexera activation.
Note: For fnp/flexera activations, the activation is always borrowed to the local computer.
Example:'130-3618734'
CodeMeter container id/mask-serial number used when borrowing a CodeMeter activation.
-bt|--borrowterm
The period of time the specified activation will be borrowed for, in the form <number of days>:<number of hours>.
You may enter multiple borrow terms so long as an equal number of other required options are also entered.
Example: '90:0' or '0:8'
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal