Rehost an activation when Internet access is not available

Rehosting an activation removes the activation from the current host and returns it to the pool of activations on the activation server.
On a computer without an Internet connection, you cannot select a quantity of activations less than the total number of activations. All activations are removed from the local computer.
If Internet access is not available, call
Rockwell Automation
Technical Support to rehost the activation file.
IMPORTANT:
CodeMeter
-based activations cannot be rehosted manually.
To rehost an activation when Internet access is not available:
  1. Click
    Advanced
    >
    Rehost Activation Manually
    .
  2. Select the checkboxes next to the activations to rehost.
  3. Click
    Complete Rehosting
    . A confirmation dialog box opens.
  4. Click
    Continue
    to remove the activation files from this computer, or click
    Cancel
    to end the process without removing the activations.
  5. Click
    Print
    to print the information for
    Rockwell Automation
    Technical Support.
  6. Call
    Rockwell Automation
    Technical Support at the number listed on the
    Complete Rehosting
    page for a guide through the steps to rehost activation files.
    To return to the
    Select Activations
    page, click
    Rehost Activation Manually
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal