Update Activation Search Path

The Activation Search Path is the location that the client computer searches when finding available activations. You can have multiple search paths. The client searches the selected paths in order. If a path is not selected, it will not be searched.
After modifying the Activation Search Path, restart the
FactoryTalk Activation
service.
The following settings are available in
Update Activation Search Path
.
Setting
Description
Path to Activations
Either a local directory path for locating activation files on the computer's hard disk drive or a server name. Selecting the checkbox includes the path in the search path list. Clearing the checkbox removes it from the list.
Add Server
Create a new, blank row in the
Path to Activation
list. Click the
Browse
button to use a folder tree to locate the computer on your network.
Delete
Removes the currently selected path from the
Path to Activation
list.
Up
Moves up the selected path one position in the list to modify the search order.
Down
Moves down the selected path one position in the list to modify the search order.
Merge to Default
Merges activations in multiple local folders to the default Activations folder. This button is only visible when more than one local folder is present in the search path.
Tip:
Clicking this button results in the activation files being copied from the previous folder to the default Activations folder. A progress dialog box opens during the copy operation. If an error occurs, the progress dialog expands to reveal a list of errors. If a file is not successfully copied, then that file's directory is not removed from the server search path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal