C - F

capacity activation
A type of concurrent activation in which the number of activations is based on some defined capacity of the product, such as tag count, number of users, or number of computers.
concurrent activation
A type of activation that allows multiple computers across a network to use Rockwell Software products at the same time. Concurrent activations include floating activations and borrowed activations.
A borrowed activation can be disconnected for the network and can be returned manually or on timeout.
dongle
A dongle is a security or copy protection device for commercial computer programs. When required by a program, a dongle must be connected to an input/output port, such as USB or parallel port of the computer, to allow the program to run. Programs that use a dongle query the port at startup and at programmed intervals thereafter, and terminate if the dongle does not respond with the expected validation code.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal