Move an activation to a computer without Internet access

After downloading activations to a removable storage device, move the activations to the computer that is not connected to the Internet.
Before you begin:
  • Download activations from an Internet-connected computer to a removable storage device.
To move an activation to a computer without Internet access:
  1. Attach the removable storage device that includes the downloaded activations to the target computer.
  2. On the
    FactoryTalk Activation Manager
    home page, click the
    Manage Activations
    tab.
  3. Click
    Get New Activations
    .
  4. Click
    I have downloaded activation files and need to move them to this computer
    .
  5. Click
    Specify File Location
    . The
    File location
    box displays the location of the file on the removable storage device. Click the
    Browse
    button to select a different location.
  6. Click
    Move Files
    to import the files and activate the licenses.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal