Bind an activation to an Ethernet MAC ID

Use the following procedure to bind an activation to an Ethernet MAC ID manually.
To bind an activation to an Ethernet MAC ID:
  1. On the
    FactoryTalk Activation Manager
    page, click
    Manage Activations
    .
  2. Click
    Get New Activations
    .
  3. Enter the serial number and product key for the product that you want to activate and click
    Validate Activation
    .
  4. (optional) For each product in the
    Validate Activation
    table, the
    Product Version
    column displays the earliest version of the product available. Use this default value or select a different version.
  5. To download more than one copy of the activation, edit the value in the
    # to Download
    cell.
  6. Click in the
    Binding
    field and enter the 12-character MAC ID as one contiguous string. Do not include spaces or colon (:) separators. For example: 0123456789AB.
  7. Click
    Download Activation
    .
  8. After the activations have downloaded, click
    Print
    to save a copy of the activation information for your records.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal