Server log file

FactoryTalk Activation Manager
generates the server log file each time an activation server is started or refreshed. The log file provides the following information:
  • License file locations
  • The binding tied to licenses
  • Type of license
  • Who has checked out or borrowed activations
  • Who has returned or stopped using activations
  • Borrow errors
  • Exclude errors
    Tip:
    The server log file is overwritten when the activation server is restarted. To keep a copy of the server log file, save it with a new name before restarting the server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal