Network connectivity failure

If there is a network failure, the following factors apply to the activation server connection:
  • The computer makes three attempts to reconnect to the activation server.
  • There is a 60-second interval between attempts.
  • There is a two-hour TCP Timeout on the local computer before concurrent activations are checked back in to the activation server.
Grace period
  • Loss of network connectivity, user configuration error, hardware failure, insufficient available activations or any other activation failure will not deny the short-term use of critical Rockwell Automation software products. When activation fails, the product will still operate for a seven-day grace period.
    A message displays for these reasons:
    • When the grace period starts
    • At four-hour intervals while the software is running under a grace period
    • Whenever the software starts under a grace period
    • When the grace period expires
    • When an activation is found and the grace period is ending
    All Rockwell Automation Software products that affect running systems provide a grace period. Products used for design (that would not halt a running system) may or may not provide a grace period.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal