Check activation server status

Use
Activation Server Status
to:
  • Verify the status of activation servers.
  • Determine if an activation server is unresponsive, needs software updates, or needs activations renewed.
To check the status of activation servers:
  1. At the right of the taskbar at the bottom of the screen, click the up arrow to show hidden icons.
  2. Click the
    Rockwell Activation
    icon FTAMtrayIcon_v406.png.
  3. Click
    Check Servers Now
    . The
    Activation Server Status
    box lists the name of the activation servers and the status of each server. A server can be in the following states:
    • Unresponsive
      . Indicates that the computer is not communicating with the activation server due to a problem with the server or the connection to the server.
    • Needs update
      . Indicates that the server is not running the latest version of
      FactoryTalk Activation
      . Contact your system administrator to install the current version of
      FactoryTalk Activation
      .
  4. Click
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal