Example Options file for individual host computers

This is an example of an Options file where:
  • RESERVE 3 RS500.exe HOST OperatorComputer1 — Reserves three activations for the RSLogix 500 product for the HOST computer OperatorComputer1.
  • RESERVE 2 RS500.exe HOST OperatorComputer2 — Reserves two activations for the RSLogix 500 product for the HOST computer OperatorComputer2.
For example:
RESERVE 3 RS500.exe
HOST OperatorComputer1
RESERVE 2 RS500.exe
HOST OperatorComputer2
This example reserves five activations. Additional activations are available to other computers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal