Decrease the maximum borrow time of an activation

Use the following procedure to decrease the maximum borrow time of a borrowed activation.
To decrease the maximum borrow time of an activation:
  1. Click the
    Advanced
    tab, and click
    File Access
    .
Click
Edit Options File
to open the Options file,
flexsvr.opt
in a text editor. If the file does not exist, you will be prompted to create one.
  1. Edit the Options file using the following as an example, which uses
    RS500.exe
    as the activation feature name for the
    RSLogix 500
    product:
    MAX_BORROW_HOURS
    RS500.exe  24
    where:
    MAX_BORROW_HOURS—
    is the option to set the maximum number of hours to borrow activations.
    RS500.exe—
    is the activation feature name for the
    RSLogix 500®
    product, for example. See the increment line in the activation file to determine the correct feature name for your product.
    24—
    is the maximum number of hours.
  2. Save the file with the name
    flexsvr.opt
    in the default folder.
  3. Restart the activation service to enable the new options.
    NOTE:
    The factory-set maximum borrow time is also in the activation file
    BORROW=
    statement. If the activation file does not contain a
    BORROW=
    statement, the product does not support borrowing.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal