Data available in an activation-related message

The Diagnostic Viewer displays the following information. Some types of data are available only for specific types of transactions. The example information in the following table is for a
borrow return
transaction type.
Data
Description
Borrow return example
Transaction
Type of action requested by
FactoryTalk Activation Manager
.
borrow return
Server
The computer that requested the transaction.
LocComp2
Feature
The activation feature/file name that is being used.
RSVSESRV.250
Version
Product version number.
3.00
Serial number
Serial number of the product.
2322888888
Other
Severity
Severity of the message such as Information, Audit, Error, Warning.
Information
Audience
Type of user and security.
Operator & Secured
Time
Date and time the diagnostic information was logged.
7/2/2015 3:14:56 PM
Location
Name of computer where the diagnostic message was generated.
RemComp1
Provider
Service that provided the data to be logged.
FactoryTalk Activation
Server
User
User domain and login name, or domain and computer name, or SYSTEM depending on the transaction type.
SYSTEM
Full Name
Full name of the logged in user, or blank.
blank
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal