File folders and extensions

The following are the default
FactoryTalk Activation Manager
file folders and file name extensions.
Default file folders
By default activation files are stored in the following location:
  • C:\Users\Public\Documents\Rockwell Automation\Activations
    Tip:
    C:
    represents the system drive letter. Your directory path might be different.
Default file extensions
File extension
Description
.lic
FlexNet
license files.
.xml
Binding file and other internal,
FactoryTalk Activation Manager
files.
.WibuCmRac
.WibuCmRaU
WIBU
data files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal