User Defined Value is over range

The User Defined Value for the program or fault mode is greater than the maximum value allowed by the device configuration.
The User Defined Value specified in the
ChX
view must fall within the range of the high clamp and low clamp values defined in the
Limits
view.
Enter a User Defined Value less than the high clamp value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal