Real Time Sample is under range
The Real Time Sample (RTS) value is below the acceptable range for the device. Enter an RTS value within the acceptable range for the selected device filter, and then select
Apply
.The valid RTS range is as follows:
Catalog Number | Valid RTS Range |
---|---|
1756-IF8H | 18...10000 |
1756-IF8IH | 15...10000 |
1756-IF16H | 11...10000 |
1756-IF16IH |
Each device filter has a different lower limit for the RTS range:
Device Filter | Low Limit |
---|---|
15 Hz | 328 |
20 Hz | 275 |
50 Hz | 115 |
60 Hz | 115 |
100 Hz | 61 |
250 Hz | 25 |
1000 Hz | 11 |
Provide Feedback