Ramp rate is over range
The specified ramp rate is higher than or equal to the maximum value of 2.5*abs (high engineering – low engineering).
Check and calculate the maximum value for your configuration, enter a ramp rate value that is lower than the maximum value, and then select
Apply
.
TIP:
To enable the output to change faster, clear the
Ramp in Run Mode
checkbox in the Limits
view for the 1756-OF8H.Provide Feedback