Invalid high signal value

Possible cause and solution:
  • The high signal value is less than the low signal value.
    Enter a high signal value that is greater than the low signal value, and then apply the change.
  • The high signal value is outside of the specified input range or output range.
    Enter a value within the specified range, and then apply the change.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal