Invalid engineering value
The high engineering value equals to the low engineering value.
The high or low engineering value is the value used in the Data input tag when the analog signal is at the value specified for
High Signal
or Low Signal
. The default value for High Engineering
is 100.0000 and for Low Engineering
is 0.0000. The valid range is from -10000000 through 100000000.Enter appropriate engineering values and apply the changes.
Provide Feedback