Invalid deadband

The deadband value is not valid. The value must be less than (High Limit – Low Limit)/2.
Check the alarm configuration, specify a deadband value that is less than the maximum value allowed, and then apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal