Invalid alarm value
The alarm values are in conflict. This error occurs in one of these conditions:
- The high high limit value is lower than the low limit value.
- The high high limit value is lower than the high limit value.
- The low limit value is lower than the low low limit value.
Modify your configuration and apply the changes.
Provide Feedback